Technical FAQs

Ask a Question

On the NSX, can I use a Frame as a Switch?

No, the Switch is a complete unit without any type of thermal protection.
The Frame is only part of a Breaker and it needs a trip unit to work.
The Frame got a opening to receive the trip opening and can't work on its own due to terminals exposure and lack of protection unit.
 
Was this helpful?
What can we do to improve the information ?