Technical FAQs

Ask a Question

What does the message PCI failed to reset, unable to open network mean?

Possible Solution:
Check the system for faulty items these could be blocking the port, eg: Process of Elimination

* Faulty dimmer
* Faulty Relay.
* Fualty PACA.

Remove the product from the application and rescan the newtork, this should bypass this issue.

Also Check CBus Forums using the link below as they is other solutions, such as Version of toolkit and Com ports need checking.
http://www.cbusforums.com/forums/index.php
 
Was this helpful?
What can we do to improve the information ?