Technical FAQs

Ask a Question

What is the sensor voltage and wiring on IC2000P+ (15483)?

The sensor voltage is 24VDC

The recommended wiring is 1.5mm2 (max 100m lenght). using 0.8mm2 is also acceptable, but the max length will be approx. 50m only.
Was this helpful?
What can we do to improve the information ?