Technical FAQs

Ask a Question

Can the XALK boxes accommodate 3 normally closed contacts?

XALK boxes can accommodate a maximum of 3 contacts.
To have 3 normally closed (NC) contacts, you need to use an XALK1xx F box with 2 NC contacts and add an NC contact part number ZENL1121.
This additional contact is installed at the back of the box.

Was this helpful?
What can we do to improve the information ?