Technical FAQs

Ask a Question

Does the SIS LABEL software, part number XBY2U, run in Windows Vista?

The "SIS Label" label creation software for Harmony XB4 and XB5 pushbutton controls has been qualified for use with Windows XP and earlier.

The XBY2U software has not been validated for use in a Windows Vista environment.

The pack supplied under part number XBY2U comprises:

  • CD-ROM with the SIS Label label creation software
  • 9 assorted sheets of precut self-adhesive labels for printing
  • 7 templates, corresponding to the various types of label sheets (sold separately)

These templates correspond to the following label types:

  • ZB6YA013, ZB6YC013, ZB6YD013,
  • XVBCY2, XVBCY1,
  • ZBY1101, ZBCY1101, ZBY4100, ZBY5100.

The templates are used to check that the texts are centred before they are printed.
Sheets ZBY4100 and ZBY5100 come with backing boards and covers to ensure the labels are correctly positioned in their holders (e.g. ZBZ32 & ZBZ33).

Please note that this software is no longer avaialble, it was made obsolete in 2016 with no replacement.
Was this helpful?
What can we do to improve the information ?