Technical FAQs

Ask a Question

Are there freewheel diodes for LC1D115 and LC1D150?

There are no freewheel diodes for LC1D115 and LC1D150 contactors with DC coils. However, it is possible to use freewheel diodes from the LC1F range. The part numbers for these diodes are as follows: LA4FDE: for 24 to 48 V; LA4FDF: for 55 to 110 V; LA4FDP: for 125 to 250 V; LA4FDV: for 280 to 440 V.
Was this helpful?
What can we do to improve the information ?