Technical FAQs

Ask a Question

Do the 250A and 125A split metered distribution boards come with meters included?

The 250A and 125A split power & lighting B boards come with two energy meters fitted ( the IEM3255 ) which has pulsed output and modbus communication.
Was this helpful?
What can we do to improve the information ?