Technical FAQs

Ask a Question

What is the cable size of the solid neutral lead on the Acti 9 vigis and RCBOs ?

Please see below neutral cable sizes

Vigi units is 8mm

RCBOs 32A or below - 2.5 mm 

RCBOs  45A - 4mm

 
Was this helpful?
What can we do to improve the information ?