Technical FAQs

Ask a Question

Are the NSX 250,160 & 100 the same size?

Yes, the frame size of the NSX 250A , 160A & 100A is the same size dimensionally, providing the number of poles is the same.

And the Dimentions W X H X D for a 2/3P  are 105 X 161 X 86 mm and for 4P are 140 X 161 X 86 mm.
Was this helpful?
What can we do to improve the information ?