Technical FAQs

Ask a Question

Can the standard distribution boards SEA9BN have the door hinged on the right?

The doors of SEA9BN Isobar distribution boards can only be hinged on the left hand side. however the heavy duty board IP55 could have the hinges on the right.

It may be possible to get a modified standard version of the door and cover by contacting our quotations team on or contacting 0870 608 8 608
Was this helpful?
What can we do to improve the information ?