Technical FAQs

Ask a Question

Is the full function test Kit (33595) a complete kit?

The 33595 is a complete test kit for NW& NT with micrologic trip unit and NS breakers with STR and micrologic tip unit, however it comes with a non uk power plug which will need to be changed to a UK one by the customer. And the referene of the compatible software is 34559. No other parts are required
Was this helpful?
What can we do to improve the information ?