Technical FAQs

Ask a Question

What is the maximum temperature at the power connections of NW & NT Air circuit breakers and switch disconnectors?

The temperature limits are listed in the attached declaration of conformity, they are maximum, not mean values, but we declare that these limits are considered taking ambient temperature mean values.

Was this helpful?
What can we do to improve the information ?