Technical FAQs

Ask a Question

What is the largest outgoer for a SEA9BN Distribution board ?

The Maximum out going circuit breaker fitted in to the board under normal conditions is 63amps iC60 circuit breaker. 
It may be possible to externally mount a iC120 circuit breaker in a extension box SEA9BNEX034N, and use lug unit SEA9TB1001 ( Qty 3 ) to take current from the board.
Maximum cable size from neutral bar is 25mm CSA.
Was this helpful?
What can we do to improve the information ?