Technical FAQs

Ask a Question

How to recover the system on the HMIGTU Series?

Recovering the System on the HMIG3U
Goals and Symptoms       
Currently, our HMIG3U is provided only with the SD Card system.
The goal of this resolution is to provide the system recovery resource that can be used to backup and recover HMIGTU Series.
Causes and Fixes       
The Backup Recovery Tool has been validated.
Attached, please find the BackupRecovery.exe and Backup Recovery User Manual

Was this helpful?
What can we do to improve the information ?