Technical FAQs

Ask a Question

Are time delay relays, timers and control relays solid state or electromechanical relays ?

All the following devices have an electromechanical relay

- Time delay relays (iRTA, iRTB,....)
- Timers (MIN, MINt, MINp,....)
- Control relays (iRCU, iRCI,...)

Except the high performace impulse relays iTL+ which is a hybrid relay containing an electromanical switch and a solid state switch in parallel.
Was this helpful?
What can we do to improve the information ?