Technical FAQs

Ask a Question

How to set up the pulsed output on PowerLogic PM5100?

Wiring the Output
The Wiring for this output is shown on page 27 of the User Guide
PM5100 Digital Output

Please refer to the documentation. Here is a link to the User Guide:
PowerLogic™ PM5100 Series Power and Energy Meter User Guide EAV15105 - EN04 02/2015
 
 
Programing the Output
Programing the Output can be done in two ways
Via the Keys on the Panel of the Meter
Via the software IONSetup
 

Programing the Output via the Keys on the Panel of the meter is shown in the Meter User Guide

Programming the PM5100 Powwer meter
Please refer to the documentation pages 47-50. Here is a link to the User Guide:
PowerLogic™ PM5100 Series Power and Energy Meter User Guide EAV15105 - EN04 02/2015

Programing Via the IONSetup Software

Digital Output Module
This is a programing task, to set up the Pulsed Output, see pages 140 to 143 of the Programing Guide.
Here is a link to the Programming Guide:
ION Reference ION Architecture & ION Modules 7EN02-0290-08 10/2016

Was this helpful?
What can we do to improve the information ?