Technical FAQs

Ask a Question

What are the pm5100 error codes?

This error code 0041 hex is for overrunning energy pulse output.

The error list is provided as below :

1. 0003 hex : RAM failure
2. 0005 : NVRAM failure
3. 0009 : RTC failure
4. 0011 : Calibration failure
5. 0031 : Clipping detected
6. 0041 : Over running energy pulse output
7. 0081 : Back up Ram/ Vbat Fail
8. 0101 : Language file incompatibility
Was this helpful?
What can we do to improve the information ?