Technical FAQs

Ask a Question

Can NW16 be fitted in a NW25 chassis?

NW16 and NW25 have the same chassis (same dimensions) but clusters configuration is different.
Withdrawable NW16 breaker can be mounted in NW25 chassis but unused clusters must be removed in order to get the same configuration as layout.
Please check attachment for more details.

Customers are not allowed to remove the clusters, pleae consult Schneider electric services team
Was this helpful?
What can we do to improve the information ?