Technical FAQs

Ask a Question

Does power launcher software work on windows 8?

Power Launcher has been validated with OS windows up to 7.
Such application embeds RSU and RCU which can be used to set and control masterpact and compact circuit breaker.
I have been told that Power Launcher  is not supposed to be supported in the future (at least for the RCU and RSU application embedded inside Power Launcher).

RCU and RSU is replaced by Ecoreach asset manager, running at the moment under Windows 7 mainly.

The validation of Ecoreach under Windows 8 will be considered.
Was this helpful?
What can we do to improve the information ?