Technical FAQs

Ask a Question

What is the maximum physical cable size allowed for CT inputs on the ION8800? and on the CM4000?

The maximum physical cable size is 12 AWG on direct connection.
Was this helpful?
What can we do to improve the information ?