Technical FAQs

Ask a Question

Is it possible to extend the neutral cable section on the A9V02763 vigi unit?

It is possible to extend this cable, we advised doing this using a crimp. The copper cable section connected and recommended for this situation is 8mm², we are aware this size is not available in the uk 10mm would be the alternative.
 

Was this helpful?
What can we do to improve the information ?