Technical FAQs

Ask a Question

What are the functions of the Telefast ABE7CPA412 sub-base?

The ABE7CPA412 Advantys Telefast sub-base is used as a wiring interface for BMXART0414 and BMXART0814 M340 automation platform thermocouple modules.

It is used to:
  • connect 4 thermocouple probes
  • perform external cold junction compensation using the temperature sensor integrated in the sub-base and ensure continuity of shielding.
 Note: The BMXART0814 module requires 2 ABE7CPA412 Advantys Telefast sub-bases.
Was this helpful?
What can we do to improve the information ?