Technical FAQs

Ask a Question

When is the Isobar neutral link used?

Neutral links are used  to link between the neutral incomer and the neutral of the outgoing device
When: 1P&N outgoing breaker is used in Isobar type A board or B board.
          4 pole outgoing breaker is used in Isobar type B board.
 
Was this helpful?
What can we do to improve the information ?