Technical FAQs

Ask a Question

What is the Breaking Capacity of iQuickPRD Type 2 or Type 3 ?

The Breaking Capacity of iQuickPRD Type 2 or Type 3 is 25KA
Was this helpful?
What can we do to improve the information ?