Technical FAQs

Ask a Question

What is the purpose of the Ethernet 499TWD01100 communication module?

The TwidoPort 499TWD01100 module is an easy-to-use Ethernet interface, designed for the Twido programmable controller, version 3.0 or later, compact or modular. It enables the Twido controller to be integrated in an Ethernet network as a passive device (slave) . Connected on the integrated RS 485 serial port of each compact or modular base, the TwidoPort interface module is a gateway between the Ethernet TCP/IP network and the Modbus serial link of the Twido controller.
The connection cable between the base and the TwidoPort module is supplied with the module.
Was this helpful?
What can we do to improve the information ?