Technical FAQs

Ask a Question

Can I access the diagnostics of an OTB island using the Advantys software?

No, there are no diagnostic functions for an OTB island in the Advantys software. 

The OTB NIM modules manage a limited number of online operations, which are as follows:
  •  Connection to the physical island.
  •  Disconnection from the physical island.
  •  Downloading the data configured in the island.
  •  Unloading the configured data from the island.
  •  Changing the connection parameters.
Was this helpful?
What can we do to improve the information ?