Technical FAQs

Ask a Question

What is the part number for the SDE contact for a Masterpact NT or NW.

The SDE contact is fitted as a standard on the Masterpact NT or NW circuit breaker.

An optional second SDE contact can be fitted to the circuit breaker if it's specified at the time of ordering.

A second SDE contact can be fitted to an existing Masterpact NT or NW by contacting the Schneider Electric service department on 01249 456045. This is necessary, as the Micrologic has to be dismantled.
Was this helpful?
What can we do to improve the information ?