Technical FAQs

Ask a Question

How can I know whether an AS-i product has standard or extended addressing?

To find out whether the addressing of an AS-i product is:
  • standard
  • extended

Simply check the value of the AS-Interface profile's second character:
  • If the value is A = extended addressing
  • If the value is anything other than A = standard addressing

For example:
  • ASI20MT4I4OR (profile S7. 0.F.E): standard addressing  
  • ASI20MT4I4E (profile S0.    A.7.0): extended addressing A/B
Was this helpful?
What can we do to improve the information ?