Technical FAQs

Ask a Question

Is Ethernet communication possible with the Zelio logic modules?

Ethernet communication is possible but only with Zelio logic modular modules supplied with 24 VDC (SR 3B... BD).  The SR3NET01BD communication extension must be used. For more information on using this module, refer to the catalogue extract attached to this documentation:
Was this helpful?
What can we do to improve the information ?