Technical FAQs

Ask a Question

What is the configuration software for Lexium 05?

The configuration software for Lexium 05 servo drives is called Powersuite.

The part number of the PowerSuite software is VW3A8104 and  there are two options for connecting a PC to the drive.

Option 1 - Serial

The part number of the connection kit for connecting the serial port on the PC running PowerSuite to a Lexium 05 drive is VW3A8106. 

Option 2 - USB

The part number for a cable to connect the USB port on a PC running Powersuite to a Lexium 05 drive is TCSMCNAM3M002P.
Was this helpful?
What can we do to improve the information ?