Technical FAQs

Ask a Question

What is the difference between the LAD93217 and LAD93218 kits and between the LAD91217 and LAD91218 kits?

The star-delta kits part numbers LAD91217 and LAD91218 are designed for LC3D09, LC3D09A, LC3D12 and LC3D12A star-delta starters.

The star-delta kits part numbers LAD93217 and LAD93218 are designed for LC3D18, LC3D18A, LC3D32 and LC3D32A star-delta starters. 

The LAD91217 and LAD93217 kits comprise the following elements:
  • power circuit connections,
  • the fixing accessories required for fixing the contactors on the plate,
  • an LADS2 time delay contact block.

The LAD91218 and LAD93218 kits are almost identical to those above but do not include the time delay contact block.

Was this helpful?
What can we do to improve the information ?