Technical FAQs

Ask a Question

How many terminal shields do the GS1AP part numbers contain?

Part numbers GS1AP33, GS1AP43 and GS1AP63 are terminal shields for 3-pole fuse switch disconnectors.

GS1AP33 for   100 - 160A rating
GS1AP43 for   200 - 400A rating
GS1AP63 for   630A rating


Part numbers GS1AP34, GS1AP44 and GS1AP64 are terminal shields for 4-pole fuse switch disconnectors.

GS1AP34 for   100 - 160 A rating
GS1AP44 for   200 - 400 A rating
GS1AP64 for   630 A rating

To provide protection upstream and downstream of the switch disconnector, two sets of GS1APxx must be ordered.

Was this helpful?
What can we do to improve the information ?