Technical FAQs

Ask a Question

How can I lock the direct rotary handle on a Compact NS400 / NS630 circuit-breaker?.

The direct rotary handle can either be locked with padlocks or a keylock.

Locking with Padlocks:
Up to three padlocks can be fitted. The shackle diameter must be between 5 to 8mm.

Locking with a keylock:
Install: a keylock adaptor (without lock), part number 32604, and either a Ronis lock, part number 41940 or a Profalux lock 42888
The locks have random key numbers and come complete with two keys.
Was this helpful?
What can we do to improve the information ?