Technical FAQs

Ask a Question

Can the Compact NSX MCCB range be used on a DC system.

No, the Compact NSX100 to 630 MCCB range cannot be used on a DC system. However, the NSX switch disconnectors can be used as Isolators.

Use the Compact NS100DC to 630DC range for DC supplies.
Was this helpful?
What can we do to improve the information ?