Technical FAQs

Ask a Question

How can I select an optional module in the configuration of a Twido PLC?

To use an optional module (TWDNAC, etc.) you need to add the module to the PLC configuration;

In TwidoSoft:
  • Right-click on "Hardware" then select the option to be added.
  • In the "Describe" tab, select the option to be added and drag it into the relevant position.
Was this helpful?
What can we do to improve the information ?