Technical FAQs

Ask a Question

How can I stop or start the XIP driver from the Windows explorer?

In the Windows explorer, launch the "NA_Config.exe" tool in 'C:\Windows\System32'.
The Driver can then be stopped as shown below:

Was this helpful?
What can we do to improve the information ?