Technical FAQs

Ask a Question

What is the part number of the cable connecting the LTMR controller and the LTMCU operator control unit?

The LTMCU operator control unit can be connected to the LTMR controller by means of three Schneider cables with the following part numbers:

VW3A1104R10, length: 1 m
VW3A1104R30, length: 3 m
VW3A1104R50, length: 5 m
For distances greater than 5 metres:

Was this helpful?
What can we do to improve the information ?