Technical FAQs

Ask a Question

What pushbutton family is recommended for installation with a 9001K type station?

For an installation with empty boxes/enclosures of the 9001KY, KYS and SKY type, the recommended family of 30 diameter buttons is 9001K.

More information on Harmony 9001 K.
Was this helpful?
What can we do to improve the information ?