Technical FAQs

Ask a Question

What is the part number of a mechanical liquid level control switch?

The legacy XL1 range of level control switches are still available and can be used for checking the level of liquids.

These are complete units, 3 versions available;

  • Float and cord control
  • Float and rod control
  • Versions are available for normal and corrosive atmospheres

Product information is not included in current Schneider catalogues.

The attached extract from a previous catalogue contains technical information to enable a selection to be made.
If you wish to purchase these products you will need to contact your local Customer Care Centre to check availability in your region.

As an alternative to a mechanical liquid level switch, the RM35 electronic level control relays may represent a solution for detection of levels;

  • Liquid level using resistive probes - RM35LM33MW
  • Liquid or solid level using discrete sensors - RM35LV14MW
Was this helpful?
What can we do to improve the information ?