Technical FAQs

Ask a Question

Can I distribute cable or satellite broadcast over the LexCom Performance (Delta 8) Home Networking System?

LexCom Performance (Delta 8)  will not transmit feeds from the LNB of a satellite receiver. To achieve the same satellite channel in multiple rooms you must use the RF output on the receiver and connect to the RF input on the LexCom Performance (Delta 8)  unit. The system will allow the use of multiple receivers within the the home
Was this helpful?
What can we do to improve the information ?