Technical FAQs

Ask a Question

What is the minimum and maximum single length I can run LexCom Performance (Delta 8) cable?

The minimum and maximum single length that can be run is  minimum of  2 metres and a  maximum of 50 metres. Cables are installed in a star configuration and should be segregated form any mains cabling.

 

A bend radius of 25mm is recommended
Was this helpful?
What can we do to improve the information ?