Technical FAQs

Ask a Question

The Programme LED flashes continuously in a pattern of 2 for 1 minute then stops on an Ulti switch / dimmer

Possible causes are

1.   A Low Voltage Halogen (12V) has blown.  Replace the lamp load if it is blown, then perform a unit reset

2.   A magnetic transformer is faulty. Check the status of magnetic transformer.
Was this helpful?
What can we do to improve the information ?