Technical FAQs

Ask a Question

XACA069SPEC0712 availability?

SPEC0712 Pendant
This product was a custom build specification for RS Components
This pendant is no longer available as it originally contained a unique contact block (ZA2BZ141) which is no longer produced and has no replacement.
The issue is that the contact block contained 3 contacts of 2 NC + 1 NO configuration and there is not a method of replicating this configuration with individual contacts as only 2 contacts may be associated with any one pushbutton in an XACA pendant.
Whilst it is not possible to create a like for like replacement in the XACA range of pendants, a build of the same function can be created in the XACB range, as this can replicate the ZA2BZ141 function using Harmony 5 components, which cannot be used in the XACA pendants.
A scheme sheet is attached for download, with a parts listing for self assembly, or send the scheme sheet to
to request a quote for us to custom build the unit for you..
Was this helpful?
What can we do to improve the information ?