Technical FAQs

Ask a Question

In what type of control station can I install control and signaling units from the Harmony style 5 range?

Harmony style 5 range (XB5) buttons can be used on the front panel of the following control stations:
  • XALK, XALD: plastic control stations,
  • XAMW: metal elbowed control stations,
  • XAPM, XAPJ, XB2SL: metal control stations,
  • XAPE: faceplates and empty flush-mounting control stations,
  • XAPA: plastic control stations,
  • XALG: control stations for severe environments.
Caution: You need to check that
  • The overall dimensions of all elements including the transformer power supplies for certain indicator lights,
  • Stacks of contacts for pushbutton and selector switch type actuators,
  • 4-direction joystick controllers,
are compatible with the depth of the cases.
Was this helpful?
What can we do to improve the information ?