Technical FAQs

Ask a Question

Can the circuit breakers type; GB2, GV2 and GV3 be mounted on DIN rail?

Yes, all the circuit breakers, regardless of rating, with part number commencing GB2, GV2 or GV3, can be mounted on 35 mm DIN rail.
Was this helpful?
What can we do to improve the information ?