Technical FAQs

Ask a Question

What are the main upgrades of the Advantys configuration software made by Version 4.0 ?

The main upgrades to the Advantys configuration software made by Version 4.0 are as follows:
  • Standardisation of the look and feel of the software.
  • To simplify configuration of the Advantys STB, OTB, FTB and FTM systems.
  • Improved I/O map for STB.
  • New information tab for STB.
  • Enhanced diagnostic data for Advantys STB modules.
  • Inclusion of a new Advantys STB EtherNet/IP network interface module NIM (STB NIC 2212).
  • Provision of TeSys T and TeSys U connectivity on CANopen STB extension.
  • Enhanced graphic editor.
  • Inclusion of all functions in the earlier versions and database upgrades.
Was this helpful?
What can we do to improve the information ?