Technical FAQs

Ask a Question

With XTEL V5 or V6, can I save a PL7-3 program under a name other than "PL7-3.bin"?

Yes, with XTEL V5 or V6, you can change the saved name of the PL7-3 binary file using the [STR. NAME] key.

Caution: This modification should only be used when archiving applications.
In fact, when transferring the application, the XTEL [Transfer] tool only recognises the application which has the name "PL7-3.bin".
It is therefore vital to rename the application as "PL7-3.bin" prior to transfer.
Was this helpful?
What can we do to improve the information ?