Technical FAQs

Ask a Question

How can I simulate an application on XBTH, XBTP or XBTE with XBTL1000 without PLC?

To simulate an XBTH, XBTP or XBTE application in XBTL1000, without being connected to a PLC, you need to: Deselect the "use the dialogue table" box in the "Dialogue Table Configuration" window, Start simulation, Enter address 0 when simulation asks you to.  It is now possible to display the page sequences without getting the error code "Cannot write table".
Was this helpful?
What can we do to improve the information ?