Technical FAQs

Ask a Question

What should I do if I lose my password on an XBTVA?

If a password is lost on an XBTVA, place a male connector in the XBT's serial link connector.
On this male connector, create a link between the following pins: 8-11-12. 
Connector: 25-pin male SUB-D connector, NFC 93425 (HE 501).
Was this helpful?
What can we do to improve the information ?