Technical FAQs

Ask a Question

How compatible are applications between XBTVA and XBTVM?

There is XBTVA to XBTVM upward compatibility.

Using XBTEL900, an application for XBTVA, and the associated configuration, can be transferred to an XBTVM.
Likewise, an EEPROM memory cartridge containing an application for XBTVA can be inserted in an XBTVM.
Note:
If the message "Test cartridge: incorrect" appears, simply press [Enter].

It is not possible to transfer an XBTVM cartridge to XBTVA.
However, using XBTEL900, an XBTVM application on its own can be transferred to an XBTVA, by answering "No" to the question "Do you also want to transfer the configuration?"
Was this helpful?
What can we do to improve the information ?